Other Parts Discussed in Thread: CSD25480F3,
Tool/software:
Hi,
We plan to use this device as a power switch in a battery operated device which is used in at temperatures up to 60°C.
It would be very helpful to know how the expected IDSS and IGSS would be at this temperature at VDS and VGS = –3V.
We are also considering optional using the CSD25480F3 as I would expect the leakage will be lower at 3V as it is designed for higher voltages.
Info: I do not need an ESD Diode in the PFET and I am only switching maximum 3mA.
Are there any estimates or measurements of the leakage at elevated temperatures available to assist in the decision?
Is there a better suitable PFET available?
Thanks
Fred