Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQSTUDIO, BQPRODUCTION
Tool/software:
Hi,
We have some 2S battery packs with BQ40Z50-R2 v2.08 that works fine. But there are some where there is serious imbalance (0.4V) between the cells. The circuit is similar to the EVM circuit.
To be free of previous error, I started a new config file (with firmware 2.08). The chemistry is set, the learning cycle was done, and the RA tables got updated. The cell balancing is enabled during rest and sleep too.
The packs are in rest now since two days, with CB is on. Cell 1 is at 3863mV, Cell 2 is at 4291mV.
But in BQ Studio, I see that "Cell 1 Current" and "Cell 2 Current" values are constantly shifting between 0 and -20mA. The imbalance between the cells remained the same after two days of balancing.
In this situation, cell 1 should not be discharged at all by the internal mosfet, right?
The config file is attached.