Tool/software:
LM5155 Boost Converter Design:-
Hi ,
I am facing heating issue of MOSFET and Schottky Diode at below mentioned I/P ,O/P parameters.
Output getting decreased after MOSFET is heating above 120 deg.
Is it thermal shutdown of LM5155 Controller? oR Mosfet? or Inductor?
Is there any other References/parameter causing heating issue???
Vin:- 8.4V to 12.6V
Vout :- 54V/ 2A
Switching Frequency:- Fsw:- 445Khz.
Inductor is 10uH/10Amp
MOsfet :- IRFB4110 100V/180A
Reference Sch:-