This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28881: Isolated flyback design - troubles with output power

Part Number: UCC28881

Tool/software:

Dear support

I'm testing my design of UCC28881 flyback voltage source. It works in case of lower input voltage cca up to 90VAC. Once it is barely reaching the requested output parameters (cca 24VDC / 0.15A), it is starting to limit switching somehow. Some protection is probably launching. There is in datashet I(limit)= 440mA. I expect that this value is RMS. I'm not reaching this limit so far. Could you please consider what is the issue? 

Thank you 

Zdenek

 SCH+Transformer.zip