This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21551-Q1: Which FIT number to use?

Part Number: UCC21551-Q1

Tool/software:

Hello!

In  https://www.ti.com/lit/fs/sffs693/sffs693.pdf table 2-1, my customer is wondering why there are 3 FIT numbers shown on the  total component FIT row? and which to use for analysis, the highest?

Thanks!

Reed

  • Hi Reed,

    These three values are the time to failure based on three different power dissipation levels: 10mW, 100mW, and 300mW. You should choose the number that is associated with the power level closest to your application use case.

    Best regards,

    Sean