Hi,
I am in the process of implementing a flyback converter for PoE using the TPS23757 chip
http://www.ti.com/product/tps23757#technicaldocuments
I am having some problems with the current sense feedback. I have my blanking time set to 120ns and a sense resistor of 0.27 ohms but as soon as the converter is turning on the voltage at the CS pin jumps to 2 volts (there is a lot of noise on it) and the converter kicks in the over current protection and shuts down as soon as the blanking time is reached. The inductance of the primary winding on my flyback transformer is 230uH and I am running the converter at 350kHz.
I noticed in some of the reference designs the CS pin is biased to 0.25 volts by pulling it high to either Vb or VDD (see figure 1 here http://www.ti.com/lit/ug/slvu318b/slvu318b.pdf ).
What is the purpose of biasing the CS pin in the reference design?
Has anyone else had issues with excessive noise appearing on the CS pin? How did you solve it? I have implemented an RC filter to try and minimize the nose but it has not helped a lot.
Cheers
Phil