Tool/software:
Hello e2e,
This question applies to a critical long duration space-flight mission.
If the PGOOD pin is pulled up to VDD/Vin=2.5V what is the behavior of the PGOOD pin during the interval when VDD/Vin is ramping up:
- PGOOD is low over entire interval while VDD/Vin is ramping ?
- PGOOD will follow VDD/Vin up to some voltage and then go low, i.e., some minimum voltage is required on VDD/Vin to guarantee PGOOD will be driven low?
- If this is the behavior, what VDD/Vin voltage level guarantees PGOOD will drive low?
- Some other behavior. If this is the case, please explain that behavior.
NOTE: VLDOIN will be Un-powered and the EN pin will be low during the interval when VDD/Vin is ramping up.
Thank you, -John