This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25970: BQ25970 Failed to enable charging

Part Number: BQ25970
Other Parts Discussed in Thread: BQSTUDIO, BQ25890, TUSB422, BQ25968

Tool/software:

Dear

    BQ25970 was debug-verified by the BQstudio tool, and it was found that the battery could not be charged after enabling charging. The register was read again, and it was found that the charging enable was disabled again.

Q2:The system adopts the combination of BQ2589x and BQ25970 fast charge scheme, how to switch the charging path?

Q3:The BQ25890 and TUSB422 PD control chips used in the system are equivalent to two fast charge protocols QC2.0 and PD. After the QC2.0 and power adapter protocols are used for the first time during the system power-up, do I need to re-plug the charging cable if I want to switch to other voltage levels through PD protocol during the charging process? The power adapter uses the BC1.2 protocol to enter the power transmission mode, and should not support the replacement of the fast charge protocol for reconfiguration.

Q4:BQ25970 chip input voltage is required to be twice the battery voltage, does it mean that VIN>2VO is enough? For example, the battery voltage is 4V, and the input can be 9V or 12V?

Q5:BQ25970 and BQ25968 are P2P compatible. Are there any other differences? At present, the specification of BQ25970 chip only has a simple system block diagram, without specific pin definition and other items, can you provide a detailed specification?