Part Number: BQ24401
Other Parts Discussed in Thread: BQ25798,
Tool/software:
Hello E2E Experts,
Good day.
I was wondering if this would be a suitable charger for solar applications.
If so I noticed on the data sheet that the schematic of the sample design notes an input DC voltage of 9-16V. However, if I were to use a 6V solar panel would this design still be functional? If so would it just charge the batteries at a slower rate? Or does the input DC voltage need to be 9V even to charge 3x 1.2V nominal NIMH batteries?
Regards,
TI-CSC