This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24075: BQ24075RGTR Charge protection time

Part Number: BQ24075
Other Parts Discussed in Thread: BQ24072

Tool/software:

hi  

  Test charge protection time  about BQ24072. The external power supply at the battery end is 3.8V, and the USB end is 5V. The battery is only connected to the NTC and GND to ensure the normal operation of the charge IC

The definition here is the Charge safety timer and the definition is 4-6H.  but 
I tested it a little off spec, 6.04H. What could be the cause?      

   Q2 :QON PIN   external Gnd, can always be in a LOW state, or will there be any impact   ?  

  Q3:I connect a capacitor to the PIN of TMR. If the capacitor is not full at the moment of power-on, will it short circuit, which will cause the timer to fail all the time?

  • Hi Liu, 

    Thank you for reaching out via E2E. Please see my comments below. 

    1) For your charge safety timer test is the TMR pin left unconnected? If not what is the resistor value between TMR and GND? Additionally was charge current constant at your set ICHG value throughout the test? I ask because charge safety timer is slowed down if at any time the device reaches the input current limit. 

    2) Can you please double check which charger IC you are referring to for Q2? The BQ24072 does not have a QON pin. 

    3) Please do not connect a capacitor to TMR pin. There should only be a resistor to GND with a value in range of 18kohm to 72kohm at TMR or pin should be left floating to set safety timer to default length. The capacitor at TMR may be impacting the result of your safety timer test. I recommend you repeat with the capacitor removed. 

    Best Regards,

    Garrett 

  • hi  Garrett

       I removed the capacitance test. Time was 6H,  It  reached the ceiling . Is there any other reason that will affect the charge protection time

  • Hi Liu, 

    To further debug please help to answer my questions from my previous reply. I have restated most critical open questions below.

    -In the new test is TMR pin left floating? 

    -What is input current limit and charge current settings in the test and have you verified charge current remains constant throughout the test? 

    Best Regards,

    Garrett

  • Hi Garrett
         new test is TMR pin left floating, input current limit is 0.5A. charge current  in the test is 472mA. See the following figure,when 6H,charge current down.

    datasheet about safty time limit max is 6H. It  reached the ceiling . Is there any other reason that will affect the charge protection time?

  • Hello, 

    Please see my comments below. 

    See the following figure,when 6H,charge current down.

    Are you stating the device stops charge or you are stopping charge? If the device is stopping charge current on its own then the safety timer appears to be working as intended. 

    Is there any other reason that will affect the charge protection time?

    All events which increase safety timer duration are listed in datasheet section 9.3.5.6. The same section also describes actions which will result in safety timer being reset. To summarize events which lead to extended safety timer are as follows:

    1) DPPM loop activated due to reaching input current limit,

    2)Charge current limited due to input voltage falling to Vin-dpm

    3)device in thermal regulation

    Best Regards,

    Garrett

  • Hi Garrett:

         the device stops charge,thank you for your reply.

    Are you stating the device stops charge or you are stopping charge? If the device is stopping charge current on its own then the safety timer appears to be working as intended. 
  • Hi Garrett:

         I have one more question,these event effcets safety timer,maybe out of range 6H? beyond specification definition 6H?

    1) DPPM loop activated due to reaching input current limit,

    2)Charge current limited due to input voltage falling to Vin-dpm

    3)device in thermal regulation

  • Hello, 

    The three events you list will all cause safety timer to count at half speed as long as they are present and therefore extend overall safety timer length. Any of those 3 events could cause safety timer to become longer than the 6 hour specification. 

    Best Regards

    Garrett