Other Parts Discussed in Thread: DRV8874,
Tool/software:
Hello;
I am designing a PCB for a single channel motor driver. Which utilizes the TPS54302 to step down 4S li on battery voltage to 5V. I don't have anything that draws too current from the converter. The design consists of an MCU, DRV8874, a CANFD transceiver, and TPS79933. I am supplying the MCU and logic supply of DRV884 from the 3.3V regulator (TPS79933) and the input will be connected to TPS54302 buck converter's output (5V).The only load directly connected to the TPS54302 will be the CANFD driver. The DRV8874 is directly connected to input voltage of the PCB.
I have checked the MCU and CANFD driver's maximum suplly currents which are 150mA and 70mA at max. and I am thinking the DRV8874's logic inputs don't consume that much current only maybe 10mA judging by the values from the datasheet.
So when I am calculating the inductor size value using the Lmin equation on the datasheet of the TPS54302 (Eq 8.) with these parameters; Iout (max) = 300mA (I took it a bit higher just to be safe) I get ınductor values like 100uH to 200uH. It seems a bit too much and even for the reference design on datasheet for 3A output it shows 10uH inductance. Am I doing something wrong here?
If you need other parameters I ll provide them.
Vin (max) = 16.8V (max voltage of 4S lion batter)
Vout = 5V (the output I want)
Imax = 300mA (output current I picked, I picked it higher than the calculation just to be safe)
and fsw of the TPS54302 says 400KHz
Thanks.