This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2825A-EP: Discrepancy of datasheet vs TI webpage

Part Number: UC2825A-EP

Tool/software:

Hello,

The UC2825A-EP TI webpage shows as device having a 50% max duty cycle. However, the datasheet shows 85% duty cycle max. Which is right?? 

  • Hi,

    There are two ways to specify the Dmax, each output and both output. The datasheet is based on both outputs together. The web is on single output. Single output way becomes popular recent 10 years or so, but before that, both outputs together way was popular. So both web and datasheet are correct. In any case, please follow the datasheet.