Part Number: UCC21530
Other Parts Discussed in Thread: TIDA-00199, UCC21551
Tool/software:
I have designed a 3 phase inverter using the UCC21530 drivers. The drivers are powered by an isolated bi-polar power supply similar to TIDA-00199. Power supply outputs are +15VDC and -8VDC relative to a reference that is tied to each high side output leg. The same outputs are also tied to a common -VDC low side reference. The configuration to drive the IGBT module are as follows:
1) UCC21530 Driver #1 - Low Side U, Low Side V
2) UCC21530 Driver #2 - Low Side W, High Side W
3) UCC21530 Driver #3 - High Side V, High Side U
The output on Driver #2 appears as I would expect. The 0 to +3.3V PWM signal from the microcontroller is amplified to +15V and -8V on the VGS pin of the IGBT module for both the Low Side W and High Side W.
The output on Driver #1 and Driver #3 seems to truncate most of the signal or not generate any signal for both the Low and High side U, and V legs.
I have tried replacing the drivers, swapping them around, removing the IGBT module from the circuit. I always end up with Driver #2 working properly and Driver #1 and #3 truncating most of the output signal. The only conclusion that I can draw is that Driver #2 works because it's amplifying a Low Side and a High Side signal whereas Driver #1 and #3 are both amplifying either a Low Side or a High Side signal.
Does anybody have an idea why I can't generate the proper output signal on Driver #1 and Driver #3?
Regards,