This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5177: LM5177 Schmatic check

Part Number: LM5177

Tool/software:

HI SIR

The attachment is my buck-boost converter circuit which used the dac to control the output value from 1~48V.

Current issues are:

  1. when EN is disabled, the output will produce 13V. When EN is enabled the Vo will reduce to 0V. 
  2. When I set the output=1V and use SMU to load 4A the circuit burned out. (3A below is ok.) 

 

Do you have any feedback for this? Thanks

buck_boost.pdf

  • Hi Chen,

    I am not sure what the circuit on the LM5177 FB is doing, what it should do and if this works as expected.

    Can you first remove this circuit and use a standard Feedback resistor divider there and check out the circuit with that.

    Best regards,

     Stefan