This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24618: BQ24618

Part Number: BQ24618

Tool/software:

Hi,

My customer is requesting help with below questions-

  1. What is the minimum input to output voltage difference required for charging a battery ?
    For example, we use a battery pack with 3x Li-ion cells (max cell-Voltage = 4.2V)
    The datasheet says that a battery is first charged to certain voltage in with constant current,
    then switches over to float charge mode (smaller current, to charge cells to the final level)

    When fully charged, our battery pack will be ideally at 3x4.2V = 12.6V.
    We have a 13V (+/-5%) power adapter feeding the battery charger.
    I am wondering whether the worst case (12.35V) power adapter voltage
    (or even the best case of 13.65V) will be sufficient to charge the battery pack.
    (Vfb input of the charger is set for battery voltage of 12.37V through Vfb voltage divider)

    Usually switching battery chargers that work as buck converters require an input voltage of 2-3V higher than that of the battery they are trying to charge.

    There is no such number specified in the datasheet (at least not that I could find, after going through the datasheet several times). All it specifies is the minimum and maximum input operating range (4.7V to 28V)
    I need someone to tell me this minimum voltage differential required. 
  2. Assuming that our power adapter output voltage is not sufficient to fully charge the battery pack to the target voltage, what will the charger IC do ?
    Will it timeout after the set duration and output status as "charging suspended" ? In our system, the battery pack charges to only about 11.4V even though the set point for battery is set to 12.37V, and the charger always ends up in charging-suspended state. 
    I am wondering the minimum input/output voltage differential is the culprit.
  3. What does the IC do if the set charging current (ISET1) can never be reached because
         there is insufficient voltage at the input (VCC pin) to deliver required charging current ?
         The datasheet says the duty cycle of the switcher can go as high as 99.5%. 
         Does it keep max duty cycle and keep going or indicate a fault condition ?
  4. In our case, by the time the battery is charged to about 55-65%, the charger enters into
        "charge suspended" mode, that indicates something went wrong. 
        But the datasheet is not clear about the conditions under which it suspends charging. 
        I see 7 conditions under which charging is disabled, but not sure these are also the conditions
        under which it enters "charging suspended" state. So, I am not clear about what pushed it to suspend charging. 


        Will it suspend charging (and indicate state as suspended) if
        a. CE input is pulled high ? or
        b.  If thermistor voltage (TS pin) moves into suspend region ? or
        c.  If the charging timer times out ?

         Is there any other reason charging could be suspended  ?

  • Hello Soumya,

    What is the minimum input to output voltage difference required for charging a battery ?

    Please refer to section 10 Power Supply Recommendations in the datasheet:

    TI recommends an input voltage of at least 1.5 V to 2 V higher than the max battery voltage.

    Assuming that our power adapter output voltage is not sufficient to fully charge the battery pack to the target voltage, what will the charger IC do ?
    Will it timeout after the set duration and output status as "charging suspended" ? In our system, the battery pack charges to only about 11.4V even though the set point for battery is set to 12.37V, and the charger always ends up in charging-suspended state. 
    I am wondering the minimum input/output voltage differential is the culprit

    Yes, it seems the minimum input/output voltage differential is the issue.

    • What does the IC do if the set charging current (ISET1) can never be reached because
           there is insufficient voltage at the input (VCC pin) to deliver required charging current ?
           The datasheet says the duty cycle of the switcher can go as high as 99.5%. 
           Does it keep max duty cycle and keep going or indicate a fault condition ?
    • In our case, by the time the battery is charged to about 55-65%, the charger enters into
          "charge suspended" mode, that indicates something went wrong. 
          But the datasheet is not clear about the conditions under which it suspends charging. 
          I see 7 conditions under which charging is disabled, but not sure these are also the conditions
          under which it enters "charging suspended" state. So, I am not clear about what pushed it to suspend charging. 

    Increasing the Input voltage will most likey resolve these issue.

    Best Regards,

    Christian

  • Hi Christian,

    I'm following up on the thread here:

    I increased input voltage (VCC) of the charger IC to 15.5V.

    Now, it should be more than sufficient to charge a battery pack to a maximum of 12.6V (three Li-ion cells/pack)
    However, even now, charging terminates at the preset voltage (through Vfb divider at the output) of 12.3V
    but then the charger still keeps switching between "suspended" and "charging" modes. 
    The following scope capture shows the charger in suspend mode for long time, dropping into "charging" mode
    for about 150mS, then going back to "suspend" mode, in an infinite loop. 
    Initially the battery voltage is about 11.25V and the charger is in suspend state.
    Then it starts charging and the battery voltage jumps to 12.275V, then charging ends and it goes back into 
    suspend mode (and battery voltage drops to 11.25V).
    It stays in suspend mode for about 1.6 seconds and starts charging again (because battery voltage drops
    below RECH threshold)


    It appears that the internal resistance of the battery has increased quite a bit (looking at the bump of 1V 
    on battery voltage while charging).
    But the charger should be toggling between "charging" and "charge complete" modes and
    NOT between "charging" and "suspend" modes.
    It is a mystery to us why the charger goes into suspend mode at all. 
    There are some conditions listed in the datasheet for the IC to go into suspend mode
    and none of those conditions are occurring in our system:

    1. charge-en (CE) is pulled high (to disable charging)(not happening)

    1. Power adapter is disconnected (UVLO, VCCLOWV or sleep mode happens)(not happening)
    2. Power input has over-voltage condition (not happening)
    3. Vref or REGN regulators (internal) are overloaded (not possible because there is no external loading on REGN and Vref regulators)
    4. IC overtemp condition (145C) happens (not possible)
    5. TS voltage (thermistor) goes out of range (i.e. battery is too hot or cold)(not possible, Vts=1.96V fixed, chrg ok)
    6. timer times out (10 hours)(but suspend happens within 
      8. Charger goes into sleep mode (VCC falls below SRN  (not happening) or UVLO condition happens (not happening)

      So, basically there is no reason for the IC to go into suspend mode, yet it keeps going in and out of suspend mode.

      With a different battery pack (with much lower internal resistance), the charger transitions from "charging" state to
      "charge complete" and never between "charging" and "suspend" states. 

      So, the higher internal resistance of the battery pack is playing some role in the charger IC going into suspend mode.
      However, the datasheet does not explain why it can go into suspend mode. 

    Thank you,

    Owen

  • Hello Owen,

    Are you using your own board or an EVM?

    If you increase the battery charge voltage limit, do you see any difference. I think the device might be entering BATOVP.

    Best Regards,

    Christian.

  • We have the charger IC on our own board, but the circuit is very similar to the one in datasheet page-27 (Figure 19).
    The battery pack (of 3x 4.2V cells) never charges to more than 11.9V even though the battery charge voltage limit is set to 12.35V
    (for a battery pack of 12.6V max), so it is not likely to go into BATOVP condition. 
    Also, when the external DC power (15V to 15.5V in this case)  is on, our system draws power from this power rail and the battery
    just gets charged if charge level is lower than what is set.
    When this condition (STAT1 constantly toggling high/low), the total duration is about 1.8 seconds, of which the charger is on for 150mS 
    and off for the remaining time. Does this 150mS have any significance to the charger IC ? 
    Looks like fast charge mode turns on, lasts for 150mS, goes off and the charger is in suspend mode, then turns on again, etc.
    I have attached another scope capture which shows that there are a few level shifts in VBAT (output of the charger going to battery).
    The red waveform is VBAT. 
    When STAT1 transitions high-to-low (charging), VBAT jumps to about 12.25V, then drops to 11.3V when STAT1 transitions low-to-high (suspend).
    But about 2/3rd way through suspend duration (about 1 second), VBAT jumps up by about 200mV, then at the end of suspend duration,
    STAT1 goes low again and charging starts again. I am not sure whether that is because it goes into precharge mode first
    (when STAT1 is still indicating suspend mode) and then goes into fast charge mode when STAT1 transitions low.
    I am not sure what determines the duration 1.85sec for the entire cycle,with the charger in suspend mode for about 1.7sec and in fast charge mode 
    for 150mSec. If VBAT reaches the set-point (through Vfb pin) it should indicate "charge complete" (STAT2=0, STAT1=1) and not "suspend"

  • Hello Anoop,


    1. charge-en (CE) is pulled high (to disable charging)(not happening)

    This should be pulled low to disable charging.

    Do you have a load on your system?

    Best Regards,

    Christian.

  • Sorry, I made a mistake with polarity of CE signal.
    What I meant is that charger can go into suspend mode if CE is driven to disable charging but that is not happening in our systems.
    In our systems, the CE pin is always high, so charging is always enabled when external PSU is providing power.
    Our system draws between 20-25 Watts, so the load is always present. But when external PSU is providing power,
    no power is drawn from battery and the battery is charged until charging is completed (or gets suspended for any reason).
    Is there any requirement as to when charging can be enabled by the system through CE pin ?
    Or can we keep it permanently in enabled state ?

    My concern is that on battery packs with higher internal resistance, the charger keeps going between charge and suspend states
    about every 1.8 seconds. It should be going to "charge complete" state and not keep toggling like this. 
    With battery packs with lower internal resistance, charging completes and the charger stays in that state. 
    I measured internal resistance of four battery packs, one known good pack vs three used packs (that were in our RMA units)
    and the failing ones have between 30% to 70%  higher internal resistance (170 mOhms vs 220-290 mOhms)
    (also, when charging gets suspended, these battery packs have open circuit voltage between 11.3V and 11.9V v/s good pack
      that charges all the way to 12.25V)
    The RMA products work fine when I insert a battery pack with lower internal resistance, indicating that there is no inherent
    manufacturing or other defect in these units, it is only the battery pack. 

    How does internal resistance of a battery pack affect the charger going into suspend state instead of charge-complete state ?

  • Hello Anoop,

    Is there any requirement as to when charging can be enabled by the system through CE pin ?
    Or can we keep it permanently in enabled state ?

    This can be permanently enabled.

    My concern is that on battery packs with higher internal resistance, the charger keeps going between charge and suspend states
    about every 1.8 seconds. It should be going to "charge complete" state and not keep toggling like this. 
    With battery packs with lower internal resistance, charging completes and the charger stays in that state. 
    I measured internal resistance of four battery packs, one known good pack vs three used packs (that were in our RMA units)
    and the failing ones have between 30% to 70%  higher internal resistance (170 mOhms vs 220-290 mOhms)
    (also, when charging gets suspended, these battery packs have open circuit voltage between 11.3V and 11.9V v/s good pack
      that charges all the way to 12.25V)
    The RMA products work fine when I insert a battery pack with lower internal resistance, indicating that there is no inherent
    manufacturing or other defect in these units, it is only the battery pack. 

    I have to debug this futher, I'm gathering more information and will provide and update after.

  • Hello Anoop,

    Can you provide your schematic?

    Best Regards,

    Christian.

  • Hello Anoop,

    Do you see this issue if you increase the input voltage?

    Can you provide a scope capture of VCC, SRN, Sysstem voltage, ACDRV, measure close to the pins.

    Best Regards,

    Christian