While using bq20z95 with 2 series cell, is it necessary to change schematic as given in SLUA465. Or it can also be done by applying external charger greater than "FLASH UPDATE OK VOLTAGE" & then changing it from 7500mV to 6000mV. After that data flash writes are enabled. In this case,do I have to make changes in circuit also as given in SLUA465 or it work fine with default ckt as given in EVM.
Regards
Deepak