Tool/software:
Hi,
I am planning to use the LP5030 to drive red laser diodes. Each laser diode has operating voltage of 2.5V and operating current of 25mA. The project will include 60 laser diodes. Is the LP5030 suitable for driving laser diodes?
I am considering whether to use two LP5030s, with each channel of them drives a diiferent laser diode. Alternatively, can I use a single LP5030 to drive all 60 laser diodes, with each channel connected to two laser diodes in parallel or in series? If so, what is the maximum number of laser diodes that can be driven by a single channel of the driver?
Thank you.