Tool/software:
Hello,
I'm trying to design a dc/dc power converter using the UCC28950 controler. The features of the converter are the following : 18V to 50V input (28V nominal), 28V and 10A isolated output.
I based my design on the one we find in the datasheet and the values available on the WeBench suggestion.
The issue I'm encountering is that at 18V input, I cannot have the 28Vout needed (at 10A). If I lower the ouput current then the converter is able to provide the 28Vout.
I tried to simulate the circuit with ideal component (mosfet and diodes), and to adjust the current sense resistors but it doesn't work...
Do you have any idea on how I can resolve my problem ?
Thanks in advance,
Florian Wallaert