Tool/software:
Hey,
I have a question about the calculation of the resistors for the voltage divider of the thermistor on page 23 of the data sheet. The values used for V_T1 to V_T5 seem inconclusive to me.
In the table for the electrical properties of the chip on page 9, these are given as a percentage of the REGN voltage. When I calculate these, however, I arrive at completely different values than those that appear to have been used in the data sheet in the calculation on page 23. If I use the values from the table, I get negative / incorrect values for the resistors RT1 and RT2. I have attached the corresponding calculations at the end of the post.
My questions are the following:
1. how do you arrive at the values for V_T1 and V_T5 from the calculation on page 23?
2. if I have interpreted the values for V_T1 and V_T5 from the table correctly, why do I get negative values for RT1 and RT2?
If I have made a mistake in the calculations or misinterpreted something in the data sheet, I would also be pleased to receive clarification in this regard :)
Best regards, Christian.