This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H1101A-SP: Output Accuracy

Part Number: TPS7H1101A-SP

Tool/software:

Hi, can you please forward me the aging information? I see several others already asking for similar info. Also, can you please extrapolate on the note 3/ as designed with 0.1% resistors? Are the resistors taken into account for the +-2%? How?

  • Hi Andrew,

    Note 3 indicates that the accuracy spec is based on characterization data that was collected with 0.1% feedback resistors but the overall spec may not capture the full statistical variation of those resistors so it may be safer to add it separately. If resistors with a larger tolerance are used for setting the output, then this will lead to larger variation of the output voltage.

    Regarding the aging data, is it ok if I contact you directly through the email you used to create your E2E account?

    Thanks,

    Sarah

  • Hi Sarah, yes you may contact me through email - thank you.

  • Thanks Andrew,

    Just emailed you. I'll go ahead and mark this thread as "TI Thinks Resolved" for now. Feel free to respond to my email if there is any clarification needed.

    All the best,

    Sarah