Tool/software:
Hi team,
My customer performed open and short cases on VCC pin of UCC21750-Q1. Would like to check with you the behavior to make sure it is aligned with device logic.
PS: VCC not share the same supply with pull up supply rail on RDY/FLT/RST.
1. VCC short to GND
When VCC short to GND, RDY pin will be pulled down for 2us, then RDY will go back to logic high.
2. VCC open
When disconnect the supply from VCC pin, we still can see 3.7V voltage on VCC pin and don't have any fault reported.
Are these phenomenon aligned?
Thanks!
Ethan Wen