This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM66200: datasheet does not directly indicate which Vout is connected to which Vin?

Part Number: LM66200
Other Parts Discussed in Thread: TPS61033, LM66100

Tool/software:

1.  Can someone tell me which Vout pin on this part corresponds to Vin1 and which Vout pin corresponds to Vin2?   This is not indicated in datasheet and I would like to use the ideal diodes independently without joining the Vouts.

2.  I will be connecting a battery on Vin1 (3.2V - 2.2V).  I will be connecting TPS61033 Boost converter to Vin2.  I will be enabling the boost converter at various times.  The ON is tied low so that the output will always be enabled.  I am looking for a sanity check here, can you foresee any reason that this might not work at switching back and forth between Vin1 and Vin2?

Sincerely

Steve