This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54424: || RE CE EMC TESTING SUPPORT || BSMA_ACMH

Part Number: TPS54424

Tool/software:

 We have completed the first level of RE CE testing of this AM6254 based EVT Board [ACM Device]. We got the negative result of these RE and CE tests. And as per report analysis we suspect that below parts can be the reason for this test failure.

1. Switcher 3V3

MPN:-TPS54424RNV
Mfr:- Texas Instrument
Sch Ref des:- U5
Test setup:-
1. CE Test Results
--> LAN1 & LAN2 CE Test POE SUPPLY MOE
Test Standard Test Mode Result Remarks
LAN1 [POE SUPPLY]
Limit: CLASS- B
Frequency: 150 KHz to 30 MHz
--> POE SUPPLY Mode
Interface:- LAN1, LAN2, USB, eMMC, RTC, Temp, IR
FAIL LAN1_CE_POE_SUPPLY_WITH_COMN-14092024
LAN2 [POE SUPPLY] FAIL LAN2_CE_POE_SUPPLY_WITH_COMN-14092024

2. RE Test Results
-->RE Test POE SUPPLY MOE
Test Standard Test Mode Result Remarks
RE [POE SUPPLY]
Limit: CLASS- B
Frequency: 30mhz To 1ghz
--> POE SUPPLY Mode
Interface:- LAN1, LAN2, USB, eMMC, RTC, Temp, IR
FAIL RE_POE SUPPLY RE-30 TO 1ghz -14.09.2024
Limit: CLASS- B
Frequency: 1ghz to 6ghz
PASS RE_POE SUPPLY_RE-1 TO 6ghz -14.09.2024

We have attached the RE & CE report and schematic design of our ACM Boards so please check and share your suggestions like what changes we should make for these components to pass this RE & CE test.

 2766.RE_POE SUPPLY RE-30 TO 1ghz -14.09.2024.Pdf2766.LAN1_CE_POE_SUPPLY_WITH_COMN-14092024.Pdf2766.LAN2_CE_POE_SUPPLY_WITH_COMN-14092024.Pdf