Other Parts Discussed in Thread: TL431, PMP10666, LM5156
Tool/software:
Dear TI Support Team,
I’m designing a flyback converter that outputs ±150V +-60mA, and while the overall circuit functions well in simulations, I’m having trouble with the soft-start function. It doesn't get activated for the first 1ms ( or untill the output voltage reaches 70V). When it activates it only works untill TL431 cathode voltage reaches 20V. I used a zener to clamp to cathode voltage at 20 volts. Soft-start function works better without the zener but TL431 cathode reaches 120 V so I need to use it. I think the problem is that when the voltage is clamped the optocoupler diode is no longer forward biased and there's no current in the transistor side so the compensation pin voltage is pulled high. I used LM5156EVM-FLY, PMP10666 and SNVC240 as reference. I used the excel document to calculate the feedback loop component values.
Thanks in advance for any advice!
Circuit parameters:
- Input: 30 V
- Output: ±150 V ±60 mA
- Frequency: 300 kHz
- Transformer turns NP:NS1:NS2 1:4:4
- Peak Current Limit 2.2 A
Schematic:

Secondary Side Feedback loop:

Output Voltage:

TL431 Reference pin:

TL431 Cathode pin:

LM5156 Compensation pin