This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2587: Step up of 35V

Part Number: LM2587
Other Parts Discussed in Thread: LM5157, LM5155

Tool/software:

We are working with LM2587ADJ some years to do step up of 35V.

We want to find a more modern replacement that will allow us to reduce the capacity of the input and output capacitors as well as reduce the size of the coil.

Design features:

  • Vin 15V to 30V
  • Vout 35V
  • Iout 3A. Inside 3A has pulses of 1A 200 microseconds