This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61440-Q1: Simulation problem with WEBENCH values

Part Number: LM61440-Q1

Tool/software:

Hello,

I used in WEBENCH this part; Input= 4V to 22V, output = 3.3V, 0.5A and got frequencies that are lower than 200KHz as defined in the datasheet.

When simulated using LM61440AFS-Q1 PSpice Transient Model: 

1. Rt has no effect on the SW waveform.

2. The output is not stable under 11V input.

Is there a problem with the WEBENCH calculations for this part?

Can I please get a PSpice simulation where the Rt works properly?

Thank you.