Tool/software:
Dear Specialists,
1. In our system, we add an external MCU to start up the TPS6521903, so we want to disable FSD and configure the EN/PB function. Will the settings be refreshed if we turn the system on again?
2. In our system, USB0 will operate only in DFU or UFP mode. Will there be an issue if we connect USB0_VBUS directly to the system 5V?
I appreciate your great help in advance.
Best regards,
Woody