This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: Seeking Advice on PWM Control of Two LEDs Using Power Mux

Part Number: TPS2121

Tool/software:

I am considering using the TPS2121 for PWM control of two LEDs.

I am looking into the circuit configuration as shown in the attached diagram, and I would like to know if there are any concerns regarding this setup.

Since the PWM will be used for the propagation of a specific signal, I want to avoid extreme distortions in the PWM waveform.
Signal Bitrate is about 9600bps. 
One concern I have is whether the SS (soft start) function might be triggered each time the circuit operates.

Could you please provide any advice or suggestions?

Thank you in advance for your help.