Other Parts Discussed in Thread: UCC21530, UCC21551, ALLIGATOR
Tool/software:
Hi
I am using UCC21530 for driving the Totem pole PFC MOSFET when the input is around 50V there are some noises seen in the output of gate driver.
Enclosed images shows the noises in the output of Gate driver When the MOSFET is connected
Switching frequency is 50kHz given from functional generator.
Duty ratio is 10%