Tool/software:
Hi exparts,
Could you tell me how to calculate PD_max under following condition?
[Condition]
The on time per pulse is 32.5 ms, and the operation as shown in the attached image is repeated at a period of 260 ms.
Three of the eight steps per channel are on (32.5 ms*3 = 97.5 ms), and two channels are on simultaneously during 1-2 phase excitation for a total of 50% of the period (32.5 ms*4 = 130 ms).
Regards,
Hiromu