Other Parts Discussed in Thread: TPS63070, TPS61033
Tool/software:
Hi team,
I have three question about this product.
①In datasheet figure 1, it is said VBAT is Powe Stage Input. In my understanding VBAT is bias input voltage(Bias VIN) said in figure 7. So figure 1 shows the efficiency when separate input voltage to VIN and Bias Vin like figure 7.
Is it correct?
②In Pspice for TI Transient model, it is said SS time can adjust by changing value of "SS_CURRENT". In my understanding, this value is internal current source value on SS or REF in 7.2 Function Block Diagram.
SS time is fixed to 2.0ms in device specific. How do I calculate start up time with SS_CURRENT value?
③Our customer is concerned about how much the efficiency on below use case. Because they want to estimate input current value.
Vin : 2.7V to 5.4V
Vout : typ 5.5V±3%
Iout : max 1A
In datasheet, there is 12V output and Iout is below 500mA situation efficiency data only. If you have efficiency data close to above use case, could you share us?
Best regards,
teritama