Other Parts Discussed in Thread: BQ28Z610, GPCCHEM
Tool/software:
Dear Sir or Madam,
We would like to ask you for help.
We are trying to use BQ28Z610 with single cell LiFePo4 cell (400mAh, 3.2V design voltage) and we are facing some issues with updating the full charge capacity on start-up of the new discharge cycle. We set up all necessary values of our systems and finished the learning procedure up to the 0x0E status. We had a lot of success in previous projects but with classical 3.7V Li-Ion batteries.
The situation is that the Cell 1 QMax is almost correctly calculated to the 460 mAh and the Full Charge capacity is set to this value somewhere during the learning cycle. But when the procedure is finished and we start the first discharge cycle the full charge capacity drops immediately to value 83 mAh (or something like this). And then for sure the gauging is not correct.
Also we have an issue seeing the FC bit set (FD is OK). Even we set up all values correctly. The used charger IC is: BQ25071QWDQCRQ1 (this charger has a little overcharge peak)
Our batteries are 2p: ENERpower 10430 LiFePo4 3.2V 200 mAh
We are using 0x4137 chem ID.
Important setting is as follows, maybe you can see some discrepancy in our setting. Attaching the Data memory export.
Many thanks for help.
1bq.gg.csv