Tool/software:
Hello,
I am using TPS25982 IC the below is the circuit diagram
While testing output short circuit condition, I am seeing negative spikes of up to 9V, like the waveform below;
As per datasheet, the maximum negative spike is -0.3V on OUT pin. I have created this transient of negative spike multiple times on the IC. IC doesnt fail.
Is it because the duration of the negative spike is very small? Is there a specification in regarding the duration of the negative transient the IC can withstand?
Even with Schottky diode, I see negative spikes upto -2V, like the waveform below.
I am interested in knowing the maximum transient duration the IC can withstand exceeding the absolute maximum ratings?
Thank you.