This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2854: Calculated frequency not matching actual frequency.

Part Number: UC2854

Tool/software:

I am using a 3300pF capacitor for Ct and a 2.8kohm resistor for Rset.  The measured frequency is ~101kHz but the calculated frequency is ~135kHz (F = 1.25/(Rset x Ct)). Why is there such a large discrepancy? The resistor has a 1% tolerance and the capacitor has a 10% tolerance.

 .