Other Parts Discussed in Thread: UCD9090
Tool/software:
Hi team,
Could you help to check the behavior?
We use GPIO18 pin 27 to monitor the power rail status. If the rails are good, the pin pulls high. If one of the rails is not correct, it pulls down.
We tried to open the one of ENA resistor to make the output voltage 0V and start up the system. The result is expected that the pin pulls down.
If we short the ENA pin to ground to make the output voltage 0V while the system has been start up, the pin still keeps high.
Is this behavior correct?
Please help to check this file.
UCD9090_Model4_20240712_V5.xml
Thanks,
Leo