This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170-Q1: LM5170-Q1

Part Number: LM5170-Q1
Other Parts Discussed in Thread: LM5170, LM5171,

Tool/software:

Hi, 

I have one doubt regarding the output voltage setting of LM5170-Q1 IC, i have seen the LM5171 is having the voltage feedback pins, but the LM5170 does not have this voltage feedback pins. So, how we can regulate the Output voltage in LM5171. Can you share some input on this. In my actual application i am using LM5171 only, but simulation i am doing with LM5170, since LM5171 does not have a simulation model.

I am working on a Tina simulation for 2 phase boost converters with LM5170 IC, here how i can fix the output voltage.

 My input voltage is 8V and output voltage expected is 14V, and the load current is 14A. If i am varying the input voltage the output voltage also will vary, how to regulate the output voltage.

Regards

Rayees K.E