This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS48111: Require only P channel MOSFET driver for precharge as a replace of BQ76200

Part Number: BQ76200
Other Parts Discussed in Thread: TPS4811-Q1

Tool/software:

I am using BQ76200 in my design currently for 48V system for driving MOSFET. 

I want to replace Charge /Discharge MOSFET with Contactor for High current application. But I want to use a Precharge circuit with MOSFET. 

Could you please help me out in selecting Driver IC for driving single Channel precharge P channel MOSFET driver on High voltage side.

My system voltage is maximum 60V.

Can you please suggest suitable options?