Tool/software:
Hi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi
Hello Mohit,
An input capacitor is not required for stability of this LDO. However, an input capacitor with an effective value of 0.47 μF minimum is recommended to counteract the effect of source resistance (especially if source impedance exceeds 0.5Ω) and inductance, which may in some cases cause symptoms of system level instability such as ringing or oscillation, especially in the presence of load transients. A higher value capacitor may be necessary if large, fast rise-time load or line transients are anticipated or if the device is located several inches from the input power source. The 1uF MLCC is recommended per good analog design practice.
Please check the recommended operating conditions table for guidance on the output capacitor. 1uF is the minimum required for stability and 2.2 uF is the recommended value for MLCC. Please account for thermal and DC bias derating when picking this capacitor.
Best regards
Ishaan