Other Parts Discussed in Thread: UCC12051-Q1,
Tool/software:
Hello expert,
Here are a few customer questions about EMI test, pls help support it:
1. The EMI test report is for UCC12051-Q1 not UCC12041-Q1 in the TI website, is UCC12051-Q1 report also suitable for UCC12041-Q1?
UCC12041-Q1 数据表、产品信息和支持 | 德州仪器 TI.com.cn
UCC12051-Q1 CISPR 25 FCC Report 2.0 (Rev. A) (ti.com.cn)
2. In the TEST report, what is the revision of CISPR 25? 2016 or 2021?
3. In the TEST report, the UCC12051-Q1 EVM can pass RE/CE Class 5 with 2pcs series Y capacitors as shown below.
What is the MPN of the Y capacitor?
Are the Y capacitors mandatory?
Can the EVM pass RE/CE class 5 if these Y capacitors are removed? Or which class can the EVM pass if these Y capacitor are removed?


Thanks!