Other Parts Discussed in Thread: BQSTUDIO, BQ76952
Tool/software:
Hi,
As I am working on a Li-Ion battery-based product design project and for the same i have chooses the BQ76942 as AFE.
The Battery has 5 series cells.
Here I have a few queries:
1) As given in datasheet example design (page no 69) for 7 series cell, we have shorted the terminals VC4 , VC5, VC6, VC7, VC8, VC9, and cell connected between the VC10-VC9, VC9-VC3, VC3-VC2, VC2-VC1 and VC1-VC0. Is it correct? Please review and comment if any.
Note: Ignore additional Provision connections for 4 series cell configuration in design (shorting provision of VC3 and VC4 through R44 and C14).
2) How many bits need to be enabled in VCELL_MODE configuration in BQstudio for 5 series cell according to the above circuit?
As per the reference document (Easy Configuration of BQ76942, BQ76952 Battery Monitors) shows the example of 8 series cell and enables the bit 10, bit 9 , bit 6, bit 5, bit 4, bit 3, bit 2 and bit 1.
While when I am doing the same for 5 cell configuration, the under-voltage protection triggers, Also on the home page of BQ studio voltage of cell 9 shows as 0V.
Kindly suggest for 5 cell configuration with the above circuit bit 9 of VCELL_MODE need to enable or not?
As per me understanding only bit 10, bit 4, bit 3, bit 2 and bit 1 needs to enable. bit 9 not required to enable in this case. Please suggest.
Thanks & Regards,
Shashikumar Rai