Tool/software:
I have configured FC_SET to be -1. Everything works as I would expect, but for one oddity. I charge the battery to 100%, then I discharge the battery to about 66% and let everything set for 2 to 3 days. When I look at the battery condition, state-of-charge is 100% and FC is set. I suspect that the battery relaxes enough for the voltage to become high-enough for the BQ34Z100-G1 to see the battery as fully charged.
Any guidance would be great.