Tool/software:
Follow-on question to my previous post on two TPS50601 devices in a tracking start-up configuration. As noted in the previous post, the customer design is set up with device #1 output = 3.3V and the second tracks this for a 1.8V output with a voltage divider between Vout1 and the SS/Track input of device #2. Voltage divider is 5K/10K.
This design basically works except the Power Good output of the second device does not come up when the output reaches 1.8V. This appears to be because the SS pin voltage only reached about 1.12V when the ramp is complete. There's a comment in the data sheet under the Power Good description (8.3.13) that indicates power good will be off if the SS/TR pin is below 1.4V.
Any ideas how we might be able to work around this? I think the only way is to change the divider to allow the SS pin voltage to reach 1.4V, but this will change the desired Ss tracking the customer is trying to meet.