Tool/software:
Hi team,
1) customer want to use LM25143, and designed in interleave mode for 500W, 24/12Vo, 41.66A, is OK to use 1 LM25143(2 phase interleave) for this design?
our product page shows Iout max it is 100Amax.
But why our webench max is only 40A for interleave design?
Even we input with 24/12Vo 40A, our webench shows “Design cannot be created”.
2) Webench show for dual output design each channel can support 40A,
for interleave should be able to design 80A, but why webench interleave option max is still 40A?
3) Can customer refer to 24V/12Vo, 30A webench schematic, and customer add more MOSFETs to increase to 42A 500W power level?
4) Because the our product page shows the Ioutmax is 100A.
If customer want to use do dual outputs design, 12Vin/ 5V and 3.3V. And both 5V and 3.3V channels are 50A.
Is it Ok for LM25143? if customer add more MOSFETs, can make LM25143 reach higher power level?
Have any concern?
Thanks