Other Parts Discussed in Thread: LM25184, LM25184EVM-S12
Tool/software:
Hi team,
We use LM25183 in the fylback circuit, and we have been tested for CE and RE (level 5), and the RE test result exceeds the standard. Here are some questions we would like to confrim with you.
1: For the RE and CE tests of LM25183, can the demo pass? Especially RE (only CE test is included in the datasheet)
2: Many measures have been tried on site, but none of them have passed. Do we have any measures to pass the RE test?
3: If the LM25183 flyback solution is difficult to pass the level 5 test, it will be changed to Boost/buck+ push-pull circuit (SN6505 or 6507)?
Requirements: Input voltage 6-18V
Isolated output voltage: 24V
Output capacity: 110mA
Best regards!
Ethan