Part Number: TPS923653
Tool/software:
Team,
Eaton is testing their LCD backlight driver using our TPS923653DRRR, see schematic below. The LCD needs 25.6V @ 40mA. The input voltage is 5V. The first issue they observed was that during open load (no LCD connected) the output of the boost converter is 63V when ADIM/HD and EN/PWM pins were pulled high. If pulled low, the device is off, so they see around 5V at the output as expected. When they connected the LCD, they pulled ADIM/HD and EN/PWM high again and saw a little smoke out of L17 (the power inductor), so they disconnected the power supply.
They are investigating why the inductor heated up that way and at the same time wanted to ask the TPS92xxx team about it. It looks like there's something wrong with the OVP. From previous conversations Eaton agreed to design Vout_max * R_OVP2 / (R_OVP1 + R_OVP2) < 1.1V. In their case Vout_Max = 25.6V since they are using the boost configuration. Rovp1 and Rovp2 were designed to provide the OVP pin with 0.5V at 25.6V.
Could it be that our device is operating with high output current mode exceeding the VCC_TH? Any feedback would be appreciated in order to help understand the root cause.

Thanks,
Tom