Tool/software:
Hi Team,
Currently, we have a product that uses BQ27426 with chem ID 3142 and a terminate of 3.5V. During the discharge process, the reading of the electricity meter may suddenly jump, for example, from 60% to 0 or from 99%. Then, by checking the parameters through the tool, it is found that the parameters have returned to their default state and entered ITPOR. Under what conditions can this situation occur.
Thank you
Best Rgards
Ziwei Wu