Tool/software:
In our design, we use the TPS548A28 chip to convert 5V to 1.0V. According to the data sheet, when Vin =0V, VCC=0V,Ven=0V, and PGOOD pulled up to 3.3V through a 10-kΩ resistor, Vpgood = 850mV~1000mV. However, after our actual test, when Vin is not equal to 0V, VCC=0V, Ven=0V, and PGOOD pulled up to 3.3V through a 10-kΩ resistor, Vpgood is still equal to 850mV. What causes this? You can refer to the following picture, where the blue line is Vin, the green line is Vpgood, the red line is Vout, and the yellow line is Ven.