Tool/software:
team,
A short circuit was found recently on the IC pin, and some IC materials might be affected by tidal waves due to a typhoon flooding in Taiwan in July!
The customer found that there were several PCB boards that were shorted when the electricity power was switched on.
Not sure if it is due to moisture or electrical issues, please help to explain and offer advice.
VCC(Pin 1) to Ground(Pin 4) => Low Impedance
Pin 8 to Pin 5 => 2.5 Ohm
Pin 7 to Pin 8 => 3.5 Ohm
Application: ups
Regards
Brian