This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV733P: soft star time

Part Number: TLV733P

Tool/software:

Hi,

I only found datasheet mentioned 1.8V/3.3V soft star time.

I would like toe know is there have TLV73325, 2.5V soft start time include typical/minimum/maximum can share to me?

Thanks!

Jeff

  • Hi Jeff,

    The soft start time for the 2.5V is the same as the 3.3V since both voltages are just gained up values of the internal reference voltage.  We do not have the min / max characterized. Typically for LDO's we expect 10-20% variation in turn on times across process variation and temperature, etc, and that's what I would expect for this device.

    Thanks,

    Stephen