Tool/software:
Hi team - Two questions:
- Is there a reason why such large bypass capacitor is needed on the VCCP pin?
- When will the simplis model be available?
Thanks,
Jacob
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team - Two questions:
- Is there a reason why such large bypass capacitor is needed on the VCCP pin?
- When will the simplis model be available?
Thanks,
Jacob
Hi Jacob,
High value of capacitor is recommended at VCCP pin of UCC25660 to help VCCP voltage not fall below the VCCStopSwitching, when the controller powered using the bias winding of LLC transformer, and the device enters burst mode. It also helps during HV startup.
I was told that the SIMPLIS model will be available in a month.
Regards
Hemanth